Visit the Industrial Automation Knowledge Base to get know-hows, hints and tips. It is designed to share vast amounts of technical knowledge and expertise in Industrial Automation products, systems, applications and markets.
The M580 makes use of DTM's to connect to Process drives, TesysT's etc. This allows for the use of IO Scanning registers on these devices through the use of Modbus Function Code 23 (might be incorrect code). I believe this is a key feature for quickly adding multiple Ethernet devices to the SCADAPack and help with advanced diagnostics on your Process network.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!