Hello SCADA & Telemetry Community,
We're pleased to announce the release of Telepace Studio 5.4.2 which provides the following SCADAPack Smart RTU Firmware versions:
• SCADAPack firmware 2.50
• SCADAPack 32 firmware 2.25
• SCADAPack 314, 33x, and 350 firmware 1.77
• SCADAPack 4203 firmware 1.77
...and a number of issue fixes. For details, please refer to the Release Notes that are available on the "Resources" tab of the Telepace Studio product page on SHOP, which is accessed using this link: <click here>
Thank you
Martin Chartrand