Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
SCADAPack E Workbench and Utilities 8.18.1 now available for download on Exchange Shop
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-03-1107:38 AM
SCADAPack E Workbench and Utilities 8.18.1 now available for download on Exchange Shop
Hello SCADA & Telemetry Community,
We are announcing that SCADAPack E Workbench and Utilities 8.18.1 is now available for download on Exchange Shop.
SCADAPack E Workbench provides an intuitive, flexible environment for developing, debugging and downloading SCADAPack E Smart RTU logic code.
New and improved features for 8.18.1 include:
SCADAPack 334E RTUs will accept a configuration for a SCADAPack 333E, 314E, 313E and 312E RTUs. When read from the RTU, the device type will report SCADAPack 334E which is the type of the actual device. This feature allows configuration files for 333E, 314E, 313E and 312E RTUs to be used with a SCADAPack 334E without modification.
Performance of some DNP3 and 60870-5-101/104 operations was improved for large point count systems.
The following Application and Firmware versions are provided in this download package:
SCADAPack E Configurator application version 8.18.1.3240
SCADAPack 3xxE Firmware version 8.18.1.241.
SCADAPack 53xE Firmware version 8.18.1.241.
SCADAPack 53xE bootloader version 1.40.
SCADAPack 3xxE bootloader version is 2.31.
To access this software download, please <click here>.