Realflo™ Flow Computer is a software solution that works in tandem with standard SCADAPack™ and latest-generation SCADAPack x70 Smart RTUs to provide gas and liquids flow measurement for well test, allocation measurement, production optimization, and well pad control. This software / hardware combination also delivers robust and cost-effective gas measurement and control in gathering, midstream, and gas transmission applications.
The current version of Realflo included for download is: 7.01.2.
Please use this link: <Click here>
Regards,
Martin Chartrand