Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] Stream ID Basic Functionality
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-10-2512:51 PM
[Imported] Stream ID Basic Functionality
>>Message imported from previous forum - Category:Trio Data Radios<< User: joelw, originally posted: 2018-10-17 18:09:28 Id:64 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
----------------------
**_jweder:_**
__________________
Stream ID's (SID's) can be used with the E, M and K Series radios to route a message from the Host to one specific Remote radio or group of Remotes. Messages going into a serial port at the Master radio will be assigned a specific Tx SID. This SID will stay with all packets sent via this port unless a Translate is done at a repeater location. In either case, the data packet will reach ALL radios which have the same SID on their Rx side. (only exception is where a repeater is set up to repeat only a limited range of SID's)
The only way to route one message so ONLY a specific RTU hears it, and the next to another specific RTU, would be to use more than one serial port. The E series have two ports for this reason. The second port can be configured to have a different Tx and Rx SID, and thus repeaters can route the packets differently.