Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
>>Message imported from previous forum - Category:Communications Products << User: mchartrand, originally posted: 2018-10-25 17:39:53 Id:257 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
_______
**_ebouthillier: We are currently using clearscada 2015 R2 with a cradlepoint IBR650E-VZ cell modem. We would like to send alarms to and operator cell phone so he can be mobile around the plant. The modem is set up with an IP address. When I try to configure the SMS pager channel I get an error that reads "(unable to connect to TCP/IP Port)". No matter what port I use. Is there set port I need to be using?_**
__________
bevanweiss: Does the IBR650E-VZ modem support a telnet AT command interface? If so, then you would want to use the port that it supports this interface on.
It would also need to support the appropriate SMS sending commands that ClearSCADA is expecting it to, which has in the past been quite an issue.