Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] Bandwidth of JR900
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-10-2503:10 PM
[Imported] Bandwidth of JR900
>>Message imported from previous forum - Category:Trio Data Radios<< User: joelw, originally posted: 2018-10-17 20:57:45 Id:105 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
---------------
**_ypinckovich: I am not much of a radio specialist but received a request from a client for some radio equipment which we are quoting with for connecting M340 plc with 2 satellite stations._**
**_We are quoting the JR900 series. If I am going to have HMIGTO and HMISTU units (6 of each) spread out over 3 locations (main building, 2 satellite panels 200 feet away), will the bandwidth be sufficient to not have much or any lag in information update?_**
**_The satellite panels will contain a couple distributed I/O with Ethernet capability and will connect to the TBURJR90000002EH0. We are choosing between TBUM297224 and TBUM297287 antennae (not sure how much power is required yet). Also, at each satellite and central panel, we will have 2 of each type of HMI panel._**
**_Thanks in advance for the help, Yarom_**
------------------------
du5tin: From the brochure the JR series can have a maximum over the air bandwidth of 512kbps, with 256 kbps being the default. Your latency time will be dependent on a lot of other factors though. At 256 kbps the typical latency for a single packet is under 100ms.