Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
72479members
328059posts

SCADAPack E Workbench and Utilities 8.18.1 now available for download on Exchange Shop

MartinChartrand
Commander Commander
Commander
0 Likes
1
336

SCADAPack E Workbench and Utilities 8.18.1 now available for download on Exchange Shop

Hello SCADA & Telemetry Community,


We are announcing that SCADAPack E Workbench and Utilities 8.18.1 is now available for download on Exchange Shop.

SCADAPack E Workbench provides an intuitive, flexible environment for developing, debugging and downloading SCADAPack E Smart RTU logic code.

 

New and improved features for 8.18.1 include:

 

  • SCADAPack 334E RTUs will accept a configuration for a SCADAPack 333E, 314E, 313E and 312E RTUs. When read from the RTU, the device type will report SCADAPack 334E which is the type of the actual device. This feature allows configuration files for 333E, 314E, 313E and 312E RTUs to be used with a SCADAPack 334E without modification.
  • Performance of some DNP3 and 60870-5-101/104 operations was improved for large point count systems.


The following Application and Firmware versions are provided in this download package:

 

  • SCADAPack E Configurator application version 8.18.1.3240
  • SCADAPack 3xxE Firmware version 8.18.1.241.
  • SCADAPack 53xE Firmware version 8.18.1.241.
  • SCADAPack 53xE bootloader version 1.40.
  • SCADAPack 3xxE bootloader version is 2.31.

 

To access this software download, please <click here>.

 

Thank you

Martin Chartrand

1 Comment
Good.