Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
72647members
328444posts

RemoteConnect™ for the SCADAPack x70 (2.6.1) now available on Exchange Shop

MartinChartrand
Commander Commander
Commander
0 Likes
0
134

RemoteConnect™ for the SCADAPack x70 (2.6.1) now available on Exchange Shop

Hello SCADA & Telemetry Community,

We are pleased to announce the release of RemoteConnect for the SCADAPack x70 (2.6.1).

 

RemoteConnect provides a flexible, easy-to-use programming and configuration environment for the SCADAPack x70 Smart RTU series, which is comprised of the SCADAPack 470, 474, 570, 574 and 575 Smart RTUs.

 

New and improved features of 2.6.1 include:

 

  • Modbus protocol can be used on USB, serial, and TCP connections for configuring, monitoring and debugging with RemoteConnect. Previously these features required using a DNP3 connection.

 

  • Added support for Modbus extended addressing to firmware and RemoteConnect. Extended addressing can be used with Modbus and Enron Modbus protocols on client and server interfaces.

 

  • Added support for support Windows 10 Enterprise (32-bit or 64-bit) - version 1909 and 2004.

 

  • Added support for Modbus multiple-bit digital object mapping in the Modbus Scanner.

 

To access RemoteConnect on Exchange Shop, <click here>

 

It is highly recommended that you review the Release Notes included in the software download itself or on the Resources Tab in Shop before installing and using this new release.

 

Thank you.

 

Martin Chartrand