Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
75348members
334588posts

EcoStruxure Geo SCADA Expert 2021 Is Now Released!

sbeadle
Sisko Sisko
Sisko
0 Likes
0
203

EcoStruxure Geo SCADA Expert 2021 Is Now Released!

Schneider Electric Software is proud to announce the release of EcoStruxure Geo SCADA Expert 2021, the newest version of our successful SCADA Host software.

Bringing increased efficiency in remote asset management, Geo SCADA Expert 2021 is a release that delivers a range of features and updates for new and existing users.

 

New Product Features


Devices and Protocols
  • SCADAPack x70 Upload – import device and point configuration from x70 devices and Remote Connect
  • Support Latest x70 and Realflo – latest x70 features and gas and fluids metering features
  • OPC-UA Client Driver – Get data from UA sources
  • IEC 61850 Driver – Communicate with IEDs (Scheduled for the January monthly release)
Redundancy During Upgrade
  • Save/sync database to old format until fully committed
  • Reduce upgrade risk
Alarm Features
  • Alarm Suppression extension – choose by condition or by database value, with release timeout
  • Alarm Persistence extension – extend persistence on advanced drivers
  • Alarm Filtering extension – allow scripting of alarm banner filters
  • Retries on IP devices – reduce alarms on poor connections
Other
  • Updated database explorer with new features
  • Virtual ViewX two factor authentication
  • And more …

 

Further Information

Please go to the Resource Center for Geo SCADA in the Schneider Electric Exchange Knowledgebase