Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
72647members
328444posts

August 2021 Updates of Geo SCADA 2020, 2019 and ClearSCADA 2017 R3

sbeadle
Sisko Sisko
Sisko
0 Likes
0
96

August 2021 Updates of Geo SCADA 2020, 2019 and ClearSCADA 2017 R3

Download all Monthly Updates for Geo SCADA 2020, Geo SCADA 2019, ClearSCADA 2017 R3 and Release Notes from the Geo SCADA Knowledgebase on Exchange here:

https://community.exchange.se.com/t5/Geo-SCADA-Knowledge-Base/Geo-SCADA-Expert-Downloads/ba-p/279115

 

Updates are a combination of our Service Pack and Hotfix releases, rolled up into a single Update for each version, inclusive of recent bug fixes and put through the latest Windows Patch testing.

 

Each Update is a full installation just like the Initial Release – which can be used to upgrade to the latest Update from a previous version (don’t forget to read the upgrade notes). It can also be used to start a brand-new installation. The Resource Center describes how to upgrade a redundant system with minimal loss of service – search for ‘Upgrade Strategy’. Separate Server, ViewX Client and Web Server hosts can be upgraded independently.

 

Get on the Mailing List

The best way to keep informed is to subscribe to this channel. Please click the blue button on the parent page of this post.

 

Other Resources

There is a discussion forum for Geo SCADA Expert users at:

https://community.exchange.se.com/t5/SCADA-Telemetry-Solutions/ct-p/scada-and-telemetry-solutions-ca...

There is a board for Geo SCADA Expert queries and also one for Telemetry Devices.

 

Of course, if you are subscribed to Geo SCADA Expert support then you can call the contact details within the ViewX About box for help.

 

Best regards,

 

The Geo SCADA Expert Team  geoscada@se.com