New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
SCADA & Telemetry Devices Forum
cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted
Lt. Commander

[import] What is Level 2 Non-Packet Modulation ?

>>Message imported from previous forum - Category:Trio Data Radios<<
User: joelw, originally posted: 2018-10-17 17:59:49 Id:60
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

----------------------

**_jweder:_**

_____________


The E Series licensed radios have a modulation type called 2 level Non Packet mode. This type is chosen under one of two circumstances.

1) The user wishes to communicate using SEL Mirrored Bits protocol. This mode reduces latency to a minimum. (approximately 7ms)

2) The user wishes to use the radio to communicate with MDS 4710B radios. (only the 4710B is supported, no other, but this is a very common type)

Certain features are disabled in this mode:
- Port B
- No Flow Control mode (Hardware Handshaking required)
- Over the air diagnostics (local diagnostics does work)
- Repeat and Translate functions (Store & Forward can be done if an external loopback plug is used)
- 128 bit AES Encryption
- Remote programming
- Collision Avoidance
- Transmit Auto on Data (must use RTS)