New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
SCADA & Telemetry Devices Forum
cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted
Lt. Commander

[import] Stream ID Basic Functionality

>>Message imported from previous forum - Category:Trio Data Radios<<
User: joelw, originally posted: 2018-10-17 18:09:28 Id:64
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

----------------------

**_jweder:_**

__________________

Stream ID's (SID's) can be used with the E, M and K Series radios to route a message from the Host to one specific Remote radio or group of Remotes. Messages going into a serial port at the Master radio will be assigned a specific Tx SID. This SID will stay with all packets sent via this port unless a Translate is done at a repeater location. In either case, the data packet will reach ALL radios which have the same SID on their Rx side. (only exception is where a repeater is set up to repeat only a limited range of SID's)

The only way to route one message so ONLY a specific RTU hears it, and the next to another specific RTU, would be to use more than one serial port. The E series have two ports for this reason. The second port can be configured to have a different Tx and Rx SID, and thus repeaters can route the packets differently.