43546members
218143posts

Which batteries to order for the Accutech Field units?

Highlighted
Lt. Commander

Which batteries to order for the Accutech Field units?

Customer support question:

I have an Accutech AI10 field unit that I'd like to use. However the battery is exhausted & I'm not sure which ones to replace it with. The existinf battery does not have a number on it identifying the type. Do you have the reference for the Accutech batteries that I should order? I found TBUM297900, but also TBUM297530 and others.

Global Training Manager
SCADA & Telemetry
1 REPLY 1
Highlighted
Lt. Commander

Re: Which batteries to order for the Accutech Field units?

Hello,
The Accutech replacement battery partnumber is actually listed on the casing itself, there is no need to open the field unit at all (only to replace the battery).

accutech.png

 

Global Training Manager
SCADA & Telemetry
Tags (2)