SCADAPack-to-cloud MQTT solution – Canada-based SI finds specialized product with technology partner
Success Stories Corner
Have a sustainability or efficiency problem? Learn how Schneider Electric is using an ecosystem approach around EcoStruxure to solve customer problems.
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
Showing results for
Show only
|
Search instead for
Did you mean:
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
JPI Solutions (SI from Canada) was looking for a solution to push data from SCADAPack RTU (Remote Terminal Unit) to the cloud using MQTT (Message Queue Telemetry Transport) protocol.
The solution
Using Schneider Electric Exchange’s contextualized search, JPI was able to discover GEN7 Systems specialized offer – SCADASuite MQTT for SCADAPack
• Unlike traditional SCADA protocols, MQTT pushes data from the field device to the host – advantages include efficient use of the communications channel and instantaneous data capture after changes (rather than waiting for the next poll).
• MQTT helps in high resolution data collection to drive advanced analyses like Machine Learning.
• MQTT helps collect data directly from SCADAPack RTUs, bypassing operational systems like SCADA.
Benefits
This collaboration between JPI Solutions and GEN7 Systems yielded mutual benefits for both the SI and the technology partner. After enjoying a free trial to test out the robust product features, JPI upgraded to a subscription to GEN7 Systems’ SCADASuite MQTT for SCADAPack through Exchange.
SI testimonial
“
“I used Exchange to execute the transaction because it was the ease of purchasing the offer directly through the platform, even in after-work hours.”