New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
SCADA & Telemetry Devices Forum
cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
Highlighted
pp
Cadet

Port function "TCP Service" in SCADAPack 575

With E-Series Configurator we can select "TCP Service" as a Port Function, which is not available in RemoteConnect.

 

For example, we have a Trio ER450 radio, its port B is currently conncted to the Port 2 (configured as TCP Service) of a SCADAPack ES for diagnostic purpose. We are upgrading the SCADAPack ES to SCADAPack 575, is there a way to migrate this function to SCADAPack 575?

 

Thanks.

1 REPLY 1

Re: Port function "TCP Service" in SCADAPack 575

The TCP service name on the Scadapack E configurator Ports and Modes setting was changed in RemoteConnect and

It is now called Terminal Server.