Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] Which location for a 900MHz yagi?
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-11-0501:00 PM
[Imported] Which location for a 900MHz yagi?
>>Message imported from previous forum - Category:Communications Products << User: mchartrand, originally posted: 2018-10-25 15:09:40 Id:219 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
_______
**_danw: The existing 900MHz yagi is mounted up tight against a steel walled building. The graphic image is in the attachment, and shows a 'looking down' view. Low signal strength between the two points requires some remedial action. Radios are 1W FHSS ethernet radios. My question is which is the best location to remount the antenna with a extended horizontal mast? The location that places some of the steel wall behind the yagi or almost no steel behind the yagi?_**
_________________
kb4mdz: Just joined the forum, and saw this question, which no one answered.
Really, I don't think it matters much. A Yagi has by its very nature a directional characteristic; signal is 'aimed' toward the narrow end. What is behind it (behind the longer, or reflector elements) has less effect.
What would be bad would be aiming the yagi parallel with the wall; and esp. close to it (within a couple wavelengths - at 900 MHz, a wavelength is about 12 inches. But that's now what you've diagrammed.