Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] What is Level 2 Non-Packet Modulation ?
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-10-2512:47 PM
[Imported] What is Level 2 Non-Packet Modulation ?
>>Message imported from previous forum - Category:Trio Data Radios<< User: joelw, originally posted: 2018-10-17 17:59:49 Id:60 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
----------------------
**_jweder:_**
_____________
The E Series licensed radios have a modulation type called 2 level Non Packet mode. This type is chosen under one of two circumstances.
1) The user wishes to communicate using SEL Mirrored Bits protocol. This mode reduces latency to a minimum. (approximately 7ms)
2) The user wishes to use the radio to communicate with MDS 4710B radios. (only the 4710B is supported, no other, but this is a very common type)
Certain features are disabled in this mode: - Port B - No Flow Control mode (Hardware Handshaking required) - Over the air diagnostics (local diagnostics does work) - Repeat and Translate functions (Store & Forward can be done if an external loopback plug is used) - 128 bit AES Encryption - Remote programming - Collision Avoidance - Transmit Auto on Data (must use RTS)