Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] Unable to run Telepace after installation.
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-11-0501:02 PM
[Imported] Unable to run Telepace after installation.
>>Message imported from previous forum - Category:SCADAPack RTU<< User: mchartrand, originally posted: 2018-10-25 15:16:18 Id:221 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
_______
**_SNaylouff: I just installed Telepace16 on a Windows 32 bit laptop and I receive the error that is attached. I have tried uninstalling and re-installing, run as admin, run in compatibility mode... I have not installed this software before and I do not know if thee are prerequisites to the installation. Am I missing something? Thanks for your help._**
Is it windows XP, vista or 7? Why do you need to run Telepace 16? Can you upgrade to a newer version? Try going directly to the .exe and run it from there. Maybe something is not handling a long file name? (looking at CONTRO~1 is the filename)
__________________________
jdale: It sounds like you are using an older version of TelePACE which was replaced by TelePACE Studio about 4 or 5 years ago.
Perhaps you are trying to install this on a Windows 7 machine. Unfortunately, the older version is not supported on Windows 7 in which case you would need to see about ordering a license for TelePACE Studio.