Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] Trio Q data radios - Selecting the correct type
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-10-2503:21 PM
[Imported] Trio Q data radios - Selecting the correct type
>>Message imported from previous forum - Category:Trio Data Radios<< User: joelw, originally posted: 2018-10-17 22:22:09 Id:116 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
---------------
**_jweder: Both the QR and QB can support the exact SAME number of remote sites. The decision to choose one or the other instead relates to how busy the channel is. This refers partially to the Transmit Duty Cycle of the Master radio. You could have ONE remote and have a very HIGH duty cycle if you poll that one site for a large amount of data, and poll it very rapidly. Or you could have 200 remotes and have a low duty cycle, if you only poll each for a small amount of data and only very infrequently. "How busy" also refers to the possibility of collisions (causing delays), and whether this is going to be acceptable or not. There are a few fairly simple questions that you should ask which might help guide the decision of choosing a QR or a QB (or a QP ) at the Master and Repeater sites:_**
Is it more important that this be a low-cost system, or more important that it be a highest-reliability system? A QR at the Master (and Repeater) site does not have the ability to work reliably at a very high transmit duty cycle, while a QB or QP at these sites can transmit constantly without over-heating. If a QR must be used at critical sites due to a limited budget then measures should be taken to ensure the transmit duty cycle is limited to approximately 20%. This can be done fairly simply in most SCADA Hosts by including a brief delay between receiving the response from one Remote and sending a message to the next Remote. There is a way to gather data on the duty cycle in the TView+ Diagnostics software package after the system has been running for some time, or the customer can simply insert a pause of perhaps 200-500 milliseconds between messages, and fine-tune that later if required.
Do you think that your system will have a lot of traffic, or will messages be less frequent? This is a fairly subjective question, and difficult to get an exact answer. But some will tell you "I need to push as much data through as possible" while others may say something like "Oh no, we only poll each site once every 10 minutes and only get a few bytes, so traffic is low." A QB or QP is the clear answer if the first is true, while a QR might be OK in the second case.
Are you able to acquire two radio frequencies, or must you work with only a single channel? If two channels (approximately 5 MHz apart) can be acquired, a QB can be used as the system's collision avoidance Master. This allows the QB to act as a "traffic cop" where it can transmit to tell other remotes to be quiet (remain idle) when it hears a signal coming in from another remote. In this way it is much less likely that two remotes will try to send messages to the Master (or Repeater) at the same time. Such a system reduces the number of collisions, which allows a busy system to operate in the most efficient manner possible. A QP won't get hot, but cannot perform the higher quality collision avoidance as can the QB, because it can only transmit OR receive, never both. But it can operate on a single channel (simplex) if that's all that the customer can get.