43545members
218143posts

[Imported] Syntax error in STF file (scadapack workbench)

Highlighted
Sisko

[Imported] Syntax error in STF file (scadapack workbench)

>>Message imported from previous forum - Category:SCADAPack RTU<<
User: PeterGroot, originally posted: 2018-10-27 10:56:30 Id:310
I cant build my solution due to this error, "**syntax error in STF file**" . I made user-defined function block then call it in the Main program. When i try to build it, the error exist. How to troubleshoot this error? And what triggers the error?

1 REPLY 1
Highlighted
Sisko

Re: [Imported] Syntax error in STF file (scadapack workbench)

>>Responses imported from previous forum


Reply From User: BevanWeiss, posted: 2019-01-03 21:11:22
Have you tried this in a fresh Workbench project.
And re-creating the UDFB maually?
Syntax error in STF file implies that the STF file is corrupt or invalid, perhaps you hand edited this file?