Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
>>Message imported from previous forum - Category:Accutech<< User: mchartrand, originally posted: 2018-10-17 19:08:09 Id:90 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
-------------------------------
**_scadaservicetech: I am looking for a driver to connect to a BR10 using CMI smart cable with model # CMI-SMARTCABLE. The one i load did not work and the universal looks different from the one from Microflex. When i connect it does not assign a com port in device manager._**
____________________
jdale: The adapter used in the CMI-SMARTCABLE was never supported on Windows Vista, Windows 7 or higher which prompted the development of the Microflex USB adapter for Accutech.
You will be better off using the Microflex universal cable or some other USB adapter that is supported with your O/S.