New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
SCADA & Telemetry Devices Forum
cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
Sisko

[Imported] SCADAPack Workbench 6 Comparison Tool

>>Message imported from previous forum - Category:SCADAPack RTU<<
User: <None>, originally posted: 2019-08-01 03:25:42 Id:479
Is there any available tool to compare SCADAPack Workbench 6 programs to highlight differences in programs?

1 REPLY 1
Highlighted
Sisko

Re: [Imported] SCADAPack Workbench 6 Comparison Tool

>>Responses imported from previous forum


Reply From User: BevanWeiss, posted: 2019-08-06 02:56:53
Unfortunately not.
If your code is ST then you can simply DIFF the appropriate logic files, but I can't remember what they are called from the top of my head, so you'd have to dive into the project folder, make a change to one (but not build) and then see which file got updated.

Once you start getting into LAD / FBD logic, the same can be done, but such DIFFs have a lot less meaning. You won't get a pretty picture from it showing the changes, just all the lines internal to the file that have changed... and a small graphical change often decimates the text content of the files.