Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
>>Message imported from previous forum - Category:Realflo Electronic Flow Measurement<< User: mchartrand, originally posted: 2018-10-17 16:53:43 Id:50 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
_________________________________________
_**bengmir: Hello, We have a SCADAPack 350 that responds with 16 bits instead of 32 bits for Long/Float registers. Could this be a configuration or firmware problem? We have a SCADAPack 330 that responds appropriately, with a firmware that is a little newer. Enron Modbus: 5001 - 6999 | Long integer 7000 - 9999 | Float Thank you for any help.**_
_________________________________________
**_bengmir: All set here, it WAS a simple setting. In RealFlo, select the communications port being used(for example, either Serial Ports or IP Configuration). There will be an Enron Modbus setting for the port which needs to be set to Enabled. The Enron Station(ID) can be set as well. Now the SCADAPack will respond with 32-bit responses for the appropriate ranges. 5000-6999 for long integer 7000-65535 for float_**