Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] Realflo Flow Extension Units
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-10-2501:16 PM
[Imported] Realflo Flow Extension Units
>>Message imported from previous forum - Category:Realflo Electronic Flow Measurement<< User: mchartrand, originally posted: 2018-10-17 18:44:02 Id:78 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
-------------------------------
**_texyank: What are the engineering units used to calculate the Flow Extension for AGA 3 gas measurement. The meter is set up to use US units of measure, psi, inches of H2O. The flow extension is reported in kg/m3s. Does the RTU do all calcs using bar and millibar? Is there a way to have the flow extension reported using the configured units?_**
__________________
PSysak: Hello,
"What are the engineering units used to calculate the Flow Extension for AGA 3 gas measurement. The meter is set up to use US units of measure, psi, inches of H2O. The flow extension is reported in kg/m3s. — Yes. It's a fixed unit in the RealFLO current readings view. RealFLO does do some conversion between the contract unit and kg/m3s.
Does the RTU do all calcs using bar and millibar? — No.
Is there a way to have the flow extension reported using the configured units? — The current RealFLO version does not support that.