43429members
217967posts

[Imported] RealFLO PC-Based Application Installation

Highlighted
Sisko

[Imported] RealFLO PC-Based Application Installation

>>Message imported from previous forum - Category:Realflo Electronic Flow Measurement<<
User: mchartrand, originally posted: 2018-10-17 19:03:19 Id:88
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

-------------------------------

**_ebret:
Can RealFLO be installed in more than one PC? The CD with RealFLO can be used to have the PC-based application installed on the field laptop as well on the engineer desktop and the maintenance desktop?_**

_____________________________

mchartrand:
RealFLO is sold as a single-user product, however, it's not licensed in any hardware or software way, meaning that from a single copy, multiple installations can be made. That being said, we don't mind if it's installed on a backup machine, but would require that multiple copies be purchased for quantities beyond that.