Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] Proper Stream ID Use with Licensed E Series Repeaters
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-10-2512:49 PM
[Imported] Proper Stream ID Use with Licensed E Series Repeaters
>>Message imported from previous forum - Category:Trio Data Radios<< User: joelw, originally posted: 2018-10-17 18:04:33 Id:62 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
---------------------
**_jweder: There is a recommended method to set up your system for the use of a repeater. This system can however cause some trouble under certain circumstances. First I'll talk about how to set up the system "normally," then discuss the alternative method._**
________________
When setting up a licensed Trio system to include a repeater, it is possible to configure the system in such a way that the initiating station hears its own message echoed back. This is never a good thing. Here's an example of the normal way to avoid this problem:
When the Repeater re-sends a message from the Master it leaves SID 1 attached. The Master itself is listening for SID 2 and thus ignores this message. When the Repeater re-sends a message from the Remote it leaves SID 2 attached. (added by the Remote) The Remote is listening for SID 1 and so ignores this message.
The only problem with this system comes when the Remote radio can sometimes hear both the Repeater and the Master. This should theoretically not happen but radio waves can be fickle. Under such a situation the Remote RTU would receive a message from the Master twice, first directly then through the Repeater. This could cause significant confusion. In such a case the Translate feature may instead be used.