Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] Problem with read/write variable in Workbench and modbus
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-10-2503:44 PM
[Imported] Problem with read/write variable in Workbench and modbus
>>Message imported from previous forum - Category:SCADAPack RTU<< User: mchartrand, originally posted: 2018-10-18 19:37:10 Id:133 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
-------------------------------
**_Josdn: I'm trying to read and write a variable via modbus to a point in the ScadaPack. In E-configurator I'm configuring a 32bit analog point which is mapped to a Modbus address. This same point is also used in my Workbench application, configured as an IO Device as RTU_RAW_WRITE. The problem I'm having is that the workbench seems to have only read access or write access, not read/write. If I configure a variable to be VarInput then it can't be writen in the program, and if I configure a variable as a VarOutput then the devices that access this point via Modbus can't write on it. How can I configure the point to be read/write?_**
_________________
bevanweiss: In ISaGRAF/SCADAPack Workbench essentially you can't.
For what you want to do, I would recommend the following: a) Configure the IO Device (In SCADAPack Workbench) as an Input (or as an output status) b) Use the OPERATE instruction anytime you want to force change the value
__________________
**_Josdn: Thanks, I'm going to try this solution._**