Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] Modbus Values from Generator
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-11-0512:57 PM
[Imported] Modbus Values from Generator
>>Message imported from previous forum - Category:SCADAPack RTU<< User: mchartrand, originally posted: 2018-10-25 14:50:30 Id:216 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
_______
**_zimmer: I am having a specific problem getting the fuel level from a decision maker 3000 generator controller. Using modscan directly connected to the generator via laptop I can get the value from register 417000 as stated in the manual for the analog input associated with the fuel level, but I cannot figure out how to use the MSIP command to get this register. Will I have to re-map it somehow to a register that the scadapack 334 can read? Thanks_**
__________________
bevanweiss:
If you're using ISaGRAF, then an IO Board should do the job. Whether your SCADApack supports ISaGRAF is unknown, you didn't say what SCADApack.
Whether Modbus RTU / TCP is unknown, you didn't say which.
The Modbus address you've typed is a 6-digit address, the older ISaGRAF v3 may not have supported this (I can't remember). ISaGRAF v5 (SCADApack Workbench 6) does for E-series SCADApacks.
_____________________
a062549: I have several of the older 3000's and I take the 40039 register (Fuel Rate* (RO WORD) /Gallons/Hour x 100 (ECM only)) and run it with a clock to figure the fuel burn and resultant fuel left scenario?