Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] JR900 Point-to-Multipoint with LinkXtend Bridge
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-10-2503:12 PM
[Imported] JR900 Point-to-Multipoint with LinkXtend Bridge
>>Message imported from previous forum - Category:Trio Data Radios<< User: joelw, originally posted: 2018-10-17 21:11:13 Id:107 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
-------------------
**_jamie8: Hi, I want to set up a master with 3 remotes. There isn't line of sight between the master and the 3 remotes so wish to add a repeater between the master and the 3 remotes. Is it possible to configure the repeater as Point to Multi-Point with LinkXtend bridge?_**
**_Then we will be able to setup dual antennas on the repeater with 1 yagi back to the master and the second a omni-directional for the 3 remotes. Or do we have to setup the repeater as an access point Point to Multi-Point and the 3 remotes as well as master as 'remotes'?_**
**_All 5 radios will be JR900-01002-EH0_**
---------------
jdale: You should be able to set up the repeater with LinkXtend bridge once you enable Antenna 2 in your repeater configuration.
In this case, the Antenna 1 port on the repeater will be used to report upstream to the master. Antenna 2 port will be used to go downstream to your remote sites.
If you are only needing one repeater using one antenna to access all sites, you can set up the repeater site as an Access Point to act as a KwikStream Repeater