Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] J Series as gateway for serial-only K Series ?
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-10-2512:43 PM
[Imported] J Series as gateway for serial-only K Series ?
>>Message imported from previous forum - Category:Trio Data Radios<< User: joelw, originally posted: 2018-10-17 17:49:53 Id:55 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
------------------------
**_sborenstein: Can the JR900 be used as a master radio and serial device server for a network of KR900's? Meaning, if I were to use a serial-ethernet converter to link to a master KR900 radio via ethernet (server to radio), can I accomplish the same task with a single JR? If so, can the JR do this for multiple streams? Steve_**
----------------------------
jweder: Hi Steve,
It is not possible for a J radio to talk directly to a K. But if you have a need to connect an ethernet device to a K (serial) network you could use an external device such as a terminal server. eg Moxa or Lantronix. However, the J Series radios now include a built-in Ethernet/serial gateway capability.