43429members
217967posts

[Imported] Isagraf Workbench

Highlighted
Sisko

[Imported] Isagraf Workbench

>>Message imported from previous forum - Category:SCADAPack RTU<<
User: mchartrand, originally posted: 2018-10-18 20:14:01 Id:138
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

-------------------------------

**_dflag:
I am currently working to replace an old RTU with Scadapack350 using Workbench for my program.I have four totalizer outputs which I mapped as modbus registers (floating points).I can read these registers in OPC but can not write to it.What Operand do you think I should use to write onto it._**

______________________

bevanweiss:
A SCADAPack RTU does not talk OPC-DA (or HDA, or UA, or XML).
So you're clearly missing details in the puzzle.