Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
[Imported] EB45e Repeater Mode
Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-10-2503:09 PM
[Imported] EB45e Repeater Mode
>>Message imported from previous forum - Category:Trio Data Radios<< User: joelw, originally posted: 2018-10-17 20:51:41 Id:103 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
--------------
**_gwapo123: I want to know if the EB45e (in repeater mode) can cater to both ER450 and ER45e over the air simultaneously with ER450 operating in serial and ER45e in ethernet mode?_**
---------------------------
jweder: The data sent over-the-air by a Trio licensed radio (any E Series or M Series radio including the Ethernet E Series) is encapsulated within a 4 byte SLIP packet in exactly the same manner. So yes, an EB45e can repeat data from either an ER450 or an ER45e.
As a related item, this also means that an EB450 (serial only type) can also successfully repeat data from either an ER450 or ER45e. It will not have some of the advanced ethernet data handling features of the EB45e however, so if traffic loading is heavy there may be more collisions. It would be preferable in such a situation as this to use an EB45e which is ethernet-aware.