43426members
217963posts

[Imported] Do SCADAPack 333E and 535E Support Time Synchronisation via IRIG-B?

Highlighted
Sisko

[Imported] Do SCADAPack 333E and 535E Support Time Synchronisation via IRIG-B?

>>Message imported from previous forum - Category:SCADAPack RTU<<
User: mchartrand, originally posted: 2018-10-18 20:15:11 Id:139
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

-------------------------------

**_Chadam:
Does anyone know if the SCADAPack 333E or 535E Support Time Synchronisation via an IRIG-B signal? If not is there a plan to release this in the near future?_**

_____________

bevanweiss:
Negative, not without additional hardware (to essentially turn IRIG-B into NTP).

The only SCADAPack item that supported out of the box IRIG-B is the SCADAPack ER with the P620 processor. I would not recommend this moving forwards.

-------------------------------

**_Chadam:
Thanks for the Reply Bevan_**