43546members
218143posts

[Imported] Cybertec SMM-200 Replacement Paging Modem having issues

Highlighted
Sisko

[Imported] Cybertec SMM-200 Replacement Paging Modem having issues

>>Message imported from previous forum - Category:Communications Products <<
User: mchartrand, originally posted: 2018-10-25 15:46:55 Id:224
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

_______

**_PaulD:
G'day,
Looking to replace a existing SMS paging modem with a Cybertec SMM-200 and when connected to ClearSCADA having a SMS Pager Channel Error - GSM Modem poll failed.
Any ideas?
I am able to send SMS via AT commands in Hyperterminal and have the SMS Channel connection settings the same as those successfully usued in Hyperterminal. I am setting ATV1E0 in the modem command.
Any help appreacited as I am already using these modems elsewhere and would prefer not to need to stock something different_**

_________

Dakshina:
Hello PaulD,

Have you had any luck with the trouble?

I am also trying to use a cybertec 2220 modem with clearscada to send sms and having exactly the same issue.

Any help would be appreciated.

________________

**_PaulD:
Dakshina,
I wasn't ablt to get the Cybertec to work as expected so ended up using a Schneider SR02 MOD02 which worked straight out of the box.
Apologies for taking so long to reply._**