43493members
218073posts

[Imported] Comunicating with Omron PLCs using Trio Data radios

Highlighted
Sisko

[Imported] Comunicating with Omron PLCs using Trio Data radios

>>Message imported from previous forum - Category:Trio Data Radios<<
User: joelw, originally posted: 2018-10-16 21:42:12 Id:35
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

-------------------------

**_ingcesarduque:
Does anyone do something like this? (Comunicating with Omron PLCs using Trio Data radios)_**

---------------------

Hello Cesar,

I am not sure what protocol the Omron PLC uses, but our Trio radios can handle virtually any normal serial or ethernet-based protocol. The packet layer in our serial-only radios can be configured to handle Modbus, DNP3 or many other protocols. If none of the choices works for you we have a Custom selection which allows you to specify how to packetize the data from your PLC's.

Joel