43426members
217961posts

[Imported] Base radio configuration lost during power outage?

Highlighted
Sisko

[Imported] Base radio configuration lost during power outage?

>>Message imported from previous forum - Category:Accutech<<
User: mchartrand, originally posted: 2018-10-17 19:34:18 Id:98
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
-------------------------------

**_Customer Question:
Is the base radio configuration retained when power is removed?_**

___________________

mchartrand:
Yes, the configuration is retained in the base radio when power is removed and reloaded when power is restored.