41521members
184571posts

[Imported] Accutech SmartCable question

Highlighted
Sisko

[Imported] Accutech SmartCable question

>>Message imported from previous forum - Category:Accutech<<
User: mchartrand, originally posted: 2018-10-17 19:21:50 Id:94
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

-------------------------------

**_Customer Question:
If I power the base radio with 12VDC, will the Accutech SmartCable function? I tried this and I don't think it does._**

_________________________

mchartrand:
No, the SmartCable gets its power from the base radio itself and requires 24VDC. So if you want to use the SmartCable Universal Interface cable, make sure the base radio is powered with 24VDC.

___________________________

AA:
The new smart cable assembly is power by the PC USB port so power is no longer an issue.