43429members
217967posts

[Imported] 4102 / 4203 tap location

Highlighted
Sisko

[Imported] 4102 / 4203 tap location

>>Message imported from previous forum - Category:Realflo Electronic Flow Measurement<<
User: mchartrand, originally posted: 2018-10-17 18:55:26 Id:85
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

-------------------------------

**_dirtydodge:
Does anyone know if the 4102 and 4203 transmitters use an "Upstream" or "Downstream" tap location for the static pressure?_**

____________________________________

mchartrand:
Hello,
They can be used for either location. The location is set in the configuration of the RealFLO flow run.