41333members
184398posts

Cybersecurity - How do you secure one millisecond latency with your solution?

Highlighted
Lieutenant JG

Cybersecurity - How do you secure one millisecond latency with your solution?

How do you secure one millisecond latency with your solution?

Tags (1)
1 REPLY 1
Highlighted
Ensign

Re: Cybersecurity - How do you secure one millisecond latency with your solution?

The point Is the following: we are using a proprietary encryption system that was for embedded micro-processors. So as the system is lightweight we can encrypt higher throughput with less resources.

 

That is important because in industrial systems it is hard to do that with a non-specific micro-processor. We can do that with off-the-shelf electronics so that basically the trick. The trick is in the mathematics.