42270members
186177posts

What does it mean by Generic Object Oriented Substation Events (GOOSE) via IEC 61850?

Highlighted

What does it mean by Generic Object Oriented Substation Events (GOOSE) via IEC 61850?

IEC 61850 defines an abstract object model for substations and methods to access these objects on a network. The abstract object model represents the SAS functionality in terms of logical nodes (LN) within the logical devices that are allocated to the IEDs as the physical devices. The actual communication between IEDs is handled via common IEC 61850 protocols such as SV, MMS and GOOSE.

 

-Ankit Acharya

Healthcare Segment KAM

Tags (1)