42268members
186168posts

How important is to follow complete IEC 61439-3 standard for LV applications?

Highlighted

How important is to follow complete IEC 61439-3 standard for LV applications?

If we follow 61439-3, we will adhere to complete system level testing. which is more closer to real time use case. There is a possibility that, products are good individually but when put in system, they behave differently and may not meet all the essential safety needs. IEC 61439-3 ensures the testing is done at system level.

 

-Ankit Acharya

Healthcare Segment KAM