42322members
212129posts

[Optimized power panel solutions for Data Centers June 10th 2020 webinar] - Is power Train same as E-House?

Highlighted

[Optimized power panel solutions for Data Centers June 10th 2020 webinar] - Is power Train same as E-House?

Question asked by Faiz

 

Can we say the Power Train is the same as E-House that we normally use in Oil & Gas applications?

Could you please show pictures of typical a Power Train, particularly the interconnection between MV to Transformer and Transformer to LV...Thanks

1 REPLY 1
Highlighted
Crewman

Re: [Optimized power panel solutions for Data Centers June 10th 2020 webinar] - Is power Train same as E-House?

A complete power train can be integrated in a container, using same technology as e-house. However, the difference between a data center and a O&G plant for instance, is that for data center, the same e-house will be used many times while an O&G plant is made a many different e-houses connected to each other.

 

Consequently from engineering and manufacturing stand point it is different. For Data center there is: 

     - less engineering using SE pre-engineered solution

     - Repetitve production of the same solution

 

Tags (1)