42311members
204641posts

EcoStruxure Power Commission: Speed up your connected power commissioning

Highlighted
Crewman

EcoStruxure Power Commission: Speed up your connected power commissioning

Check out interesting features in our software that help you commission connected power equipment faster.

 

  1. Test remote communication for system integrators at site

 

 

2. Specifically test if the circuit breaker status (open / closed / tripped) is communicated correctly on the remote communication channel

 

 

2 REPLIES 2
Highlighted
Administrator

Re: EcoStruxure Power Commission: Speed up your connected power commissioning

Hello @adityachangi,

 

Thanks for sharing this with the community members!

Best,
Firdous - Animation and Moderation Exchange Community Team
Highlighted
Lieutenant

Re: EcoStruxure Power Commission: Speed up your connected power commissioning

Hello,

 

Is Power Commission also compatibel with Windows Server 2016.

 

I have a server with PME and would like to install PC to update the drivers of the nsx, ife, MTZ,..

But after the installation I get an error that some drivers are not installed and i need to reinstall PC...

 

In the manual they do not mention windows server 2016...

 

2020-07-01 10_59_45-Window.png

 

Br,

 

Koen

Tags (1)