Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
72400members
327850posts

Why is Power Connection Integrity Such a Hot Topic?

Omaelk
Administrator Administrator
Administrator
0 Likes
0
795

Why is Power Connection Integrity Such a Hot Topic?

Even power connections that are perfectly installed tend to loosen over time; avoiding this can head off serious problems. Our previous post in this series discussed how important it is for installers to use the correct torque when tightening power connections, and some of the reasons these connections are prone to loosening over time. In this post, we explain why keeping the power connection tight is so important, and what happens without this type of protection. Read here our full blog article on "Why is Power Connection Integrity Such a Hot Topic?" here