Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2020-07-17 01:35 AM . Last Modified: 2021-10-27 11:03 AM
Posted: 2020-07-17 01:35 AM . Last Modified: 2021-10-27 11:03 AM
IEC 61850 SAS with station bus (around 2005): The IEC 61850 family of substation communication systems standards were released in the early 2000s. These standards promoted Ethernet based bay level (between bay and station level) and process-level (between switchyards and control rooms) connections using common protocols. The IEC 61850 based SAS started implementing station bus according to IEC 61850 standard. IEC 61850 SAS with station and process bus (around 2015): The IEC 61850 based SAS implements process and station bus according to IEC 61850 standard
-Ankit Acharya
Healthcare Segment KAM
Posted: 2020-08-21 03:37 AM
Thanks for those explanations, Ankit.
Any reference documentation or link to reference documention or presentation to be shared?
Posted: 2020-08-21 03:37 AM
Thanks for those explanations, Ankit.
Any reference documentation or link to reference documention or presentation to be shared?
Posted: 2021-04-28 02:23 AM
IEC 61850 in last decade provided improvement in DataPoint Quality Management (supposing evolution of IEC 61131-3), agnostic (com+electric) Configuration, fast automations (FLS 30ms DI to DO), distributed automation and standardised IED environment levels.
More recently IEC61850 has opên the path to other standards;
Ethernet seamless redundancy PRP/HSR (IEC 62439)and architecture,
fast CT/VT transmission (IEC61869)...
then new protection/control scheme like for hospital and dat Centers ASR (Automatic Self Reconfiguration), low cost directional overcurrent (sharing limited number of VT)
BR
User | Count |
---|---|
57 | |
23 | |
19 | |
16 | |
11 | |
11 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.