Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80776members
346798posts

What’s the communication performance of SAS with IEC61850

Solved
Ankit_Acharya
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
927

What’s the communication performance of SAS with IEC61850

All the IEDs were configured as per their intended run time functionality. For example, real IED1 receives binary inputs from the external world. Upon receiving the binary input, IED1 triggers GOOSE message to another real IED2. It also sends the same message to simulated IED as well. With fully functional setup, the tools captured the bandwidth utilization and transfer time for one of the messages on network. Hence, the bandwidth utilization and message transfer time is within limits and satisfactory.

 

-Ankit Acharya

Healthcare Segment KAM

Tags (1)

Accepted Solutions
Nedjma
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
834

Re: What’s the communication performance of SAS with IEC61850

Thanks for those explanations, @Ankit_Acharya.

 

Any reference documentation or link to reference documentation or presentation to be shared?

See Answer In Context

Tags (1)
1 Reply 1
Nedjma
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
835

Re: What’s the communication performance of SAS with IEC61850

Thanks for those explanations, @Ankit_Acharya.

 

Any reference documentation or link to reference documentation or presentation to be shared?

Tags (1)