Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80776members
346797posts

How important is to follow complete IEC 61439-3 standard for LV applications?

Solved
Ankit_Acharya
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
930

How important is to follow complete IEC 61439-3 standard for LV applications?

If we follow 61439-3, we will adhere to complete system level testing. which is more closer to real time use case. There is a possibility that, products are good individually but when put in system, they behave differently and may not meet all the essential safety needs. IEC 61439-3 ensures the testing is done at system level.

 

-Ankit Acharya

Healthcare Segment KAM


Accepted Solutions
Nedjma
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
830

Re: How important is to follow complete IEC 61439-3 standard for LV applications?

Thanks for sharing this information @Ankit_Acharya.🙂

 

Any reference documentation or link to reference documentation or presentation to be shared?

 

See Answer In Context

Tags (1)
1 Reply 1
Nedjma
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
831

Re: How important is to follow complete IEC 61439-3 standard for LV applications?

Thanks for sharing this information @Ankit_Acharya.🙂

 

Any reference documentation or link to reference documentation or presentation to be shared?

 

Tags (1)