Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80827members
346902posts

Evolution in IEC 62271-100 (expected publication in 2021)

Solved
Ankit_Acharya
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
1000

Evolution in IEC 62271-100 (expected publication in 2021)

Standard is getting updated for the solidly earth system for SC test duties. It is defining the additional test requirement for solidly earth system during 100% rating of symmetrical earth fault ( TD100S) and asymmetrical earth fault (TD100a).

Implications of this to on our product is to make sure that our interrupting system is withstanding the electrical stresses developed during this specific case.

Most of the our end customers ( Healthcare, Home/Buildings) will have the solidly / resistance grounded systems. This will mandate us to validate our product as per the new standard.

 

- Ankit Acharya

Healthcare Segment KAM

Tags (1)

Accepted Solutions
Nedjma
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
887

Re: Evolution in IEC 62271-100 (expected publication in 2021)

Hello @Ankit_Acharya

 

Thanks for sharing this information.🙂

 

 

 

See Answer In Context

Tags (1)
1 Reply 1
Nedjma
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
888

Re: Evolution in IEC 62271-100 (expected publication in 2021)

Hello @Ankit_Acharya

 

Thanks for sharing this information.🙂

 

 

 

Tags (1)