Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
75378members
334638posts

2020 Product of the Year Gold Award! Square D Model 6 motor control center with ArcBlok

JeffMMiller
Lt. Commander Lt. Commander
Lt. Commander

2020 Product of the Year Gold Award! Square D Model 6 motor control center with ArcBlok

Schneider Electric's Square D Model 6 MCC with ArcBlok technology has won Electrical: Fuses, Circuit Breakers, Safety Gold Award in the 2020 Consultant-Specifying Engineer Product of the Year awards.

 

ArcBlok isolates the line side conductors and reduces the likelihood of accidental contact with those conductors and the potential for arc faults.

What You Need to Know

  1. ArcBlok reduces energy released and the potential for damage.
  2. ArcBlok is a passive technology reducing negative consequences of human error.
  3. ArcBlok reduces the arc duration and self-extinguishes it in less than one cycle!
  4. ArcBlok has been tested and assessed using ANSI/IEEE Std. C37.20.7-2017, Annex H Motor Control Centers (UL 845).
  5. ArcBlok is less costly than arc resistant MCC construction and provides operational resiliency that arc resistant gear does not.
  6. ArcBlok comes with additional features for even more benefits!

 

Read more about it here